7/20/2018 2:04 PM | |
Joined: 4/8/2016 Last visit: 8/30/2024 Posts: 133 Rating: (45) |
Hello Boost34, i just checked the newest version of the PAC Library (V2.1) and it is released for PCS 7 V8.1 and hence should be compatible with all other libraries which are released for PCS 7 V8.1. But if you are saying that you are using the old PCS 7 library V6.1 with PCS 7 V8.1, you might encounter problems, because V6.1 of this library is not tested/released with PCS 7 V8.1 Only V7.1 SP3 Upd2 and V7.1 SP3 Upd3 of the PCS 7 library are tested and released with PCS 7 V8.1 So no one can tell you if there might be any conflicts, because this combination is not tested/released. For compatibility questions like this, check the compatibility tool: https://support.industry.siemens.com/kompatool/ So I think the best way now is to make a library update. |
Last edited by: 51N3P at: 7/20/2018 2:06:25 PMKind regards |
|
7/20/2018 2:31 PM | |
Joined: 3/28/2017 Last visit: 7/8/2024 Posts: 79 Rating: (0) |
Hi 51N3P, To upgrade the library I probably need a full stop of AS which I cant do. |
Last edited by: Boost34 at: 7/20/2018 2:31:27 PM |
|
8/14/2018 1:31 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi Boost34, more information about mixing the visualization of AS blocks from different PCS 7 versions on one OS client you can find in the manual "SIMATIC Process control system PCS 7 Software update without utilization of new functions" under the section "Mixed operation and visualization of AS blocks from different PCS 7 versions". I hope it will help you. With regards |
Follow us on