4/12/2016 5:08 PM | |
Joined: 12/20/2006 Last visit: 9/22/2024 Posts: 37 Rating: (0) |
I'd like add more then one trend on the Faceplate in one Trend view. How can I do it? I have an example with two trends, but I can't do it. Best Regards ziemson ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/13/2016 11:06:04 AMNew subject after splitting ziemson, |
|
4/13/2016 4:29 PM | |
Joined: 8/3/2009 Last visit: 9/23/2024 Posts: 13753 Rating: (1737)
|
Hello ziemson As I told ln my screenshots in Topic: https://support.industry.siemens.com/tf/de/en/posts/112713/ in the second Screenshot you can see that you have to set the Trandy outsinde the Faceplate at the Interface not Inside! Bye Murof |
Last edited by: The Helping Hand at: 4/13/2016 4:32:14 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/15/2016 12:56 PM | |
Joined: 8/3/2009 Last visit: 9/23/2024 Posts: 13753 Rating: (1737)
|
Hello ziemson So I give it a last try to explain. look at the Video in the Attachment: I hope you understand now Bye Murof Attachment20160415_122026.zip (733 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
9/24/2019 8:18 AM | |
Joined: 6/24/2015 Last visit: 9/17/2024 Posts: 10 Rating: (1) |
Dear Sagar, It is already editable in faceplate edit view of trend. |
Follow us on