11/3/2012 10:24 AM | |
Joined: 3/25/2008 Last visit: 4/3/2024 Posts: 240 Rating: (2) |
Hello to all, i have a problem with installation of additional driver supplyed by siemens . The driver is for redundant I/O LB/FB by Pepperl & Fuchs. I have an old project developed by ex collegues, and now i nedd to do a modify. My system is Windows XP sp2 -- S7 V5.5 -- CFC V7.1 sp2 - SCL V5.3 I open the charts correctly but if i try to do a compilation a worning is emitted : "A version for the driver library has to be selected" If i try to do a selection my combobox is empty !! I have follow step by step the instruction ( se below ) and i do not understand where is my error anyone can help me ? Thank you ------------------------------------------------- In the same manual i found that need a license maybe that's why it does not work ? My chief tell me that the driver has been regularly purchased by Siemens and probably the license is at the customer. I have only the copy of software found in my server. Now I can not ask myex colleague. No longer works with my company and I do not know where to find it. Will ask the customer, but I do not want to look bad Fom manual: 1.1 License The license is required for use of the driver blocks in a plant. ---------------------------------------------- Here an extract of the manual ( attach a entire manual ) 2.4 Driver wizard files For the CFC feature „Generate Module drivers“, the delivered XML-Files have to be copied in the following folder: <Installation path>SIEMENS\STEP7\S7data\Driver. The delivered file „PuF_LBFB_PCS7V71.reg“ has to be executed one time before using this feature. AttachmentPCS7v71_P&F_LBFB_V7.3_e.pdf (99 Downloads) |
11/6/2012 1:23 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
Hello Capraloris Did your company buy the driver in past? If this is right, then it is no problem to phone the Siemens hotline and tell them, that you have lost the licences. Tell them your order number and you will get a new license key. By the way, you can also write a mail to the Siemens customer support. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo2&aktprim=99&lang=de -> Then press "Support Request" |
Last edited by: Thunderstorm at: 11/6/2012 1:28 PMSIMATIC PCS 7 - Overview |
|
Follow us on