12/15/2015 2:40 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hi, 1.) the adress of Drive_1 is the right, or would you sen the data to the control unit? 2.) Which fatal error? If you have question to SFC14/15 refer this FAQ:
Christoph |
Last edited by: ChristophD at: 12/15/2015 2:42:59 PMLast edited by: ChristophD at: 12/15/2015 2:45:34 PM |
|
1/5/2016 8:40 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Hi. Long Time no See. I'm Trying to active Motor by PLC.... But Error makes me sad.. I think it is by ethernet. In photo1, It Is MPI, there Are caution, there are no Problems. Configuration Is good. It So strange. So I changed Access Point. But there are one caution. What i have to choose as 'Access Point' and 'PG/PC interface'? And When I use router, Do I use IP S110(192.168.0.1) OR router IP(192.168.0.6). Plus, What Is Access Point? and In PG/PC Interface, What Is main? PLC or Target? Thank you.
AttachmentPhotos.zip (96 Downloads) |
1/5/2016 10:13 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Thank you! In Photo, I tried to assign device name and IP, But there are error. What makes error? By H/W configure? AttachmentPhotos (2).zip (107 Downloads) |
1/5/2016 1:35 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
But the icons are black and have '?' And, I Use SIENES telegram 102 PZD-6/10, Not Standard, Is It ok? |
1/5/2016 1:51 PM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Thank you very much! Have a nice day |
Follow us on