5/22/2014 5:09 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Dadoui FB 2 P_RCV? In this block is not present the data type BYTE, however if you want to transfer the data type BYTE write L DB5.DBB0 T DB6.DBB0 Make sure you have created the data block DB5 and DB6. |
Last edited by: Ste39 at: 5/22/2014 5:11 PM |
|
5/22/2014 6:42 PM | |
Posts: 25 Rating: (0) |
I have this when runing CPU : attachment
Attachmentcapture.pdf (275 Downloads) |
5/22/2014 6:53 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Initially DB5.DBX 0.0 is TRUE and DB6.DBX 0.0 is False After running CPU, DB6.DBX 0.0 should be True but it 's not. Any suggestions ? I have this when runing CPU : attachment Attachment:capture.pdf (2 Downloads) So , there is a solution the first puzzle.You have used wrong operation based on language selection in SIMATIC Manager.To have more option for future go to Options-->Customize-->Language.Select English/English that is much easier for us to trace. As the attachment shows, as you are using check and assignment, your codes working perfectly.Content of RLO (VKE) is TRUE in first line and it is copied to target "DB6.DBX 0.0" in the 2nd line.Try use watch tables for more clarity.Also you can switch to LAD by using CTRL+1 for an easier view to interpret.
|
Last edited by: hdhosseini at: 5/22/2014 6:56 PM |
|
Follow us on