7/7/2017 9:44 PM | |
Posts: 13 Rating: (0) |
Hallo, i have download a new step 7 programs to a simatic 300 cpu-315- pn/dp. My profinet is fine, but my profibus not. I have 2 profibus (salve) nodes in my HW configurstion and one off them will be installed after few weeks so, only a master and one slave for now. After download and a GSD file problem i get some more faults, please see attached file for more information from the diagnostics. Installed: OB1, OB32, OB82, OB86, OB122. Is that normal situation beacouse i dont have the second profibus node yet? If yes how can i run the rest of the system with out errors until i install the second node? If not, what can be the couse of this problems? Thanks in advance. ------------------------------------------------------------------------------------------ AttachmentProfibusCommunication.docx (87 Downloads) |
Last edited by: Manthos at: 7/7/2017 9:50:22 PMLast edited by: Jen_Moderator at: 7/10/2017 10:23:34 AMNew subject after splitting |
|
7/10/2017 8:41 AM | |
Posts: 13 Rating: (0) |
Goedmorning, I add the 3 NW's and change the profibus node number, i also add SFC12 and VAT1. look attached file. would work like this? AttachmentMonday.doc (73 Downloads) |
Follow us on