9/20/2010 11:34 AM | |
Posts: 4 Rating: (0) |
Hi, Anybaody can give the sollution for the following, In my PC i am using winCC v6.2 sp2, and when i am installing wincc web navigator v6.2 sp3 it gives setup error that " NO WINCC V 6.2 SP2 INSTALLED". But in my PC winCC v6.2 sp2 already installed and i am using for long time. since i am getting setup error i couldn't install the web navigator. By Kanti Splitted from SMC 30 DATA TO SCADA/PC?? . |
Last edited by: O_Moderator at: 9/20/2010 1:53 PMnew subject after splitting |
|
9/13/2023 5:43 PM | |
Joined: 4/4/2020 Last visit: 4/17/2024 Posts: 13 Rating: (0) |
So, did you get an answer?
|
9/15/2023 8:55 AM | |
Joined: 8/3/2009 Last visit: 4/19/2024 Posts: 12816 Rating: (1634)
|
Hello the User Kanti has left the community and this Topic is about 13 years old, so you would not get an answer. If you have a problem or question about WinCC then please create an own new Topic. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on