8/12/2013 8:51 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hello, Can you try to download a "test" project to OP17 (using ProTool). Does it work? Best regards, Wizard |
8/12/2013 9:01 AM | |
Posts: 29 Rating: (0) |
Dear Mr.Wizard, where i find "test" project? |
8/12/2013 9:31 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hello, Please have a look at the following link: Why is the connection interrupted while transferring a project with ProTool to an OP? Are you using a 'Real' Com port? (COM1 or COM2) you can not use a USB-Serial convertor Best regards, Wizard |
8/12/2013 9:39 AM | |
Posts: 29 Rating: (0) |
Dear Mr.Wizard, yes, i am using COM-1 for the communication. |
8/12/2013 10:18 AM | |
Posts: 29 Rating: (0) |
Dear Wizard, Yes, after changing baud rate 38400 to 9600, now its communicating with OP and the test project downloaed on the OP 17 - DP 12. |
8/12/2013 10:37 AM | |
Posts: 29 Rating: (0) |
But after restore backup using prosave,OP17 screen still stayed at "SIMATIC V1.03 Ready for transfer" |
Follow us on