9/15/2017 6:50 PM | |
Joined: 10/19/2014 Last visit: 4/19/2024 Posts: 3 Rating: (0) |
Hello Sirs, I am facing a problem with PLC Sim v13. First I downloaded the PLC Sim v13 SP2 setup from the below link: https://support.industry.siemens.com/cs/document/109745155/simatic-step-7-including-plcsim-v13-sp2-trial-download?dti=0&lc=en-US After installation, when I checked the installed software it shows me PLC Sim v13 SP1 (see attached screenshot). I do not understand why is it so. My Step7 version is Step7 Professional v13 SP2 and I also use WinCC Professional v13 SP2. My computer configuration is Windows 7 Professional 32 bit. I created a raw project in TIA portal and tried to simulate S7-1500/1200 CPU but when I try to download the project in simulated CPU it says no device has been found. I can see in PLC sim that no IP address is assigned to the CPU. I re-installed all the software one by one but the problem remains the same. When I tried to simulate the PLC in v13 (without service pack) it worked but after upgrading the software version it failed to work for me. I am concerned if I am using correct version of PLC Sim and the link is a valid one or not. If not, please provide me other link. Also, if somebody have encountered such an issue then please guide me to a solution. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/18/2017 10:23:59 AMNew subject after splitting |
|
Follow us on