8/2/2018 7:23 PM | |
Posts: 4 Rating: (0) |
Hi people, this is my first topic on the forum. I'm Brazilian and i work as a plc programmer. Well, my questions is - [snip] 2 - I have a problem with a test I'm doing. When i do the download the hardware and software to PLC, the PLC lights the SF led. My hardware is a CPU 151-8 pn/dp with one KTP700 basic connected by profinet. They are in the same ip range. The error that appears is - Stop due to I/O error Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/3/2018 12:19:17 PMNew subject after splitting. Division of questions into separate topics. |
|
8/9/2018 1:24 PM | |
Posts: 4 Rating: (0) |
Hi, thanks for your answer. I solved the problem.... Was the servemodule (I forgot that kkkkk) that I did not connected to the cpu. Best Regards |