6/6/2017 10:13 AM | |
Posts: 41 Rating: (0) |
Hello experts. I have a SINUMERIK 840D NC version V4.4, HMI--MMC103 V4.4, ,,5 axis milling m/c second hand machine. when I post out a program I get the following errors on my screen. alarm 12550 alarm 14011 I get these alarms when I run these codes. I think I'm missing some files or my system dont support these commands. I'm new to programming in Siemens and I dont have any ideas what these codes are used for. so if anyone can give a small description what the codes do I would be very thankful. I've attached pictures from my GUD pages it only shows value on MGUD page 1 and 3 no values just empty page, also I have looked for a definitions folder but I dont have that. in my standart cycle folder I see many cycle files like cycle81 and so on but I dont have a cycle800 I have a cycle840 and when I wanted to make my first cycle81 it was not loaded witch I find weird. is there somewhere else I should load something or change a MD setting before I can get the machine to read the above lines? N120 $MA_COMPRESS_POS_TOL[X] = _camtolerance*1.2 N130 $MA_COMPRESS_POS_TOL[Y] = _camtolerance*1.2 N140 $MA_COMPRESS_POS_TOL[Z] = _camtolerance*1.2 N150 $MA_COMPRESS_POS_TOL[C] = _camtolerance*12 N160 $MA_COMPRESS_POS_TOL[B] = _camtolerance*12 N170 NEWCONF N180 FGREF[C]=10 FGREF[B]=10 N340 COMPCURV N380 ORIAXES N560 COMPOF Ill be grateful for any information that can help me get moving in the right direction regards flemming AttachmentGUD screen pics.zip (65 Downloads) |
Follow us on