1/9/2009 12:03 PM | |
Posts: 4 Rating: (0) |
Hello, I have found a FAQ:ALARM 25050 "Contour monitoring" during spindle positioning. I hope this helps regards wichtel |
1/9/2009 4:06 PM | |
Posts: 8 Rating: (1) |
Thanks Gebhardt Karl 840D ( 810D, 840D ?) (Simodrive, Sinamics ?) --- -- SIMODRIVE > when I move in jog x axis the next failure "alarm 25050 contour monitoring" > I got reset and try again to move it but the failure continued. What does it, when you turn with Feedrate 50% ? Work it now ? ----------- NO it doesn’t work , neither 50% or 2% Have the Motor from the X-Axis a Brake ? yes it has. If yes, open the Brake. I will ckeck this. |
Last edited by: peterman at: 1/9/2009 4:09 PM |
|
1/12/2009 9:32 PM | |
Posts: 8 Rating: (1) |
we switched the motor and drive(control unit and power unit) X axis for theYaxis and the alarm continued on X axis 25050contour monitoring |
1/13/2009 1:15 PM | |
Posts: 62 Rating: (5) |
Hi: Did it test the mechanical system? They are all the components in order, or maybe the geometry is not correct... Regards Marcelo Lazzaroni MS_LAZZ |
1/14/2009 2:27 PM | |
Posts: 8 Rating: (1) |
Sinumerik 840D I can't check the geometry because justmove in jog the X axis and the alarm 25050 contour monitoring appear |
1/29/2009 5:23 PM | |
Posts: 8 Rating: (1) |
Thanks everbody I could resvole this alarm, itwas a mechanical problems (back lash) into gearbox and pinion |
Follow us on