Industry Online Support
Technical Forum
10/30/2013 7:14 AM | |
Posts: 461 Rating: (29) |
This link will help u... U cant directly configure a DI for alram.. Use bit to byte conversion for converting ur DI or D0 to MW then assign this MW for the alarm.. For ex m0.0 to m1.7 under MW0 ( u can create text for every single bits that has to be displayed in the ALARM)
Wish u the same Regards, Nelliyan.G |
Last edited by: Nelliyan randy at: 10/30/2013 7:16 AMDiwali Last edited by: Nelliyan randy at: 10/30/2013 7:15 AM |
|
10/31/2013 8:36 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread How to configure Discrete Alarm in wincc flexible? Best regards O_Moderator |
Follow us on