4/3/2006 1:47 PM | |
Posts: 33 Rating: (2) |
OK. But are we have to connect the PLC ? Is it work with Simulator? |
4/3/2006 2:00 PM | |
Posts: 1084 Rating: (72)
|
Hi, no you don't need a plc to be connected. With the use of the simulator and the internal tags you should be able to generate some alarms. |
4/3/2006 2:23 PM | |
Posts: 33 Rating: (2) |
Thanks, but i can't connect to the data server yet as write on the control when running ! OOff, i want to go theparadise ! There is no Alarm Control... [:cry:] |
4/3/2006 3:29 PM | |
Posts: 33 Rating: (2) |
Maybe you going to give exactly explanation, then should not be difficult [:(] |
4/3/2006 5:02 PM | |
Posts: 1084 Rating: (72)
|
Happy to hear that it is solved. [:D] |
4/4/2006 3:40 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Guess I misunderstood [:blush:] Glad you have it working and welcome to the forum. |
Follow us on