9/27/2013 10:59 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hallo, I think the HMI KTP600 should be supported. Which firmware version is loaded the CPU 1511, V1.0 or V1.1? I recommend to make an update to V1.1, in the hardware configuration and by the real CPU. After compile and save your projekt and load the configuration in the CPU again. See also the informations in the FAQ: http://support.automation.siemens.com/WW/view/de/58522603 Mit freundlichem Gruß |
Follow us on