(1)| 11/24/2006 6:19 PM | |
|
Posts: 66 Rating:
|
Hia All! Any ideas out there? I struggeling and can't find the reason, and stat up on the plant is on Monday! Best regards Vidar |
| 12/4/2006 9:53 AM | |
|
Posts: 1398 Rating:
|
Hi SP4 can be ordered from this link. It is a simple upgrade but you will need to upgrade any optional packages you are using (see this linkfor details). The recommended method of developing a running system is to use an Engineering Station (ES) - much the same as PCS7 does. Changes should be made on the ES and then downloaded to the server while it is still running. This way you do not need to restart runtime on the server nor mess around with log files. If you have a separate spare machine then I would recommend you implement an ES as this should make life a lot easier. It does require an extra WinCC licence for the ES machine but this is a small price to pay for a working, recommended system. Salma |
Follow us on