4/10/2008 11:09 PM | |
Posts: 130 Rating: (1) |
I was under the impression you NEEDED a flash card to enable logging. Am i incorrect here? My only successes have been after adding a flash card. |
4/11/2008 5:27 AM | |
Posts: 21 Rating: (0) |
\\ isthe Root directory of the HMI. If you go to explorer and type \\ for the address, you will see the root. I had also created a folder @ \\logs but that did not work either. I will try to get a SD card today and see if that makes a difference.. Thanks, Daniel |
4/11/2008 6:13 AM | |
Posts: 21 Rating: (0) |
Just tried with one of the SD cards from our camera and it's working. |
4/11/2008 12:44 PM | |
Posts: 218 Rating: (28) |
Hi, I believe atm it is only possible to log on SD/CF-card and ethernet. I do no think you can log directly on the panel. Good to see you got it working...:D |
Follow us on