1/12/2006 4:56 PM | |
Posts: 3149 Rating: (171)
|
Hi kitofix, well, first I´d install on my system a newer PCS7 SP: http://support.automation.siemens.com/WW/view/en/19160867 Are there any strange messages in the WinCC - diagnose log files? You can find them on your PC at c:\program files\siemens\wincc\diagnose Are there entries in your "station configuration editor" > register "diagnose"? regards, Nemo |
1/27/2006 5:06 PM | |
Posts: 3 Rating: (0) |
Hello, after lookink into the files at the suggested path,here's a part of the file SIMATIC_S7_Protocol_Suite_01 located in C:\Program Files\Siemens\WinCC\Diagnose: 2006-01-13 13:18:07,390 INFO Log starting ... 2006-01-13 13:18:07,390 INFO | LogFileName : c:\Program Files\SIEMENS\WINCC\Diagnose\SIMATIC_S7_Protocol_Suite_01.LOG 2006-01-13 13:18:07,390 INFO | LogFileCount : 3 2006-01-13 13:18:07,390 INFO | LogFileSize : 1400000 2006-01-13 13:18:07,390 INFO | TraceFlags : c4000000 2006-01-13 13:18:07,390 INFO S7 channel DLL started! 2006-01-13 13:18:07,390 INFO S7 channel with own cycle creation! 2006-01-13 13:18:07,750 INFO S7DOS release: @(#)TIS-Block Library DLL Version R6.0.0.0-REL-BASIS 2006-01-13 13:18:07,750 INFO S7DOS version: V6.0 / 0 2006-01-13 13:18:07,750 INFO S7CHN version: V6.0 / Apr 30 2004 / 17:05:20 2006-01-13 13:18:07,750 INFO S7 channel unit "Named Connections" activated! 2006-01-13 13:18:13,234 ERROR Cannot connect to "APS": Errorcode 0xFFDF 410E! 2006-01-13 13:19:16,796 INFO S7 channel unit "Named Connections" deactivated! 2006-01-13 13:19:17,234 INFO S7 channel DLL terminated! APS is the name of the S7-400-FH system declared in the "Named connections" directory of WinCC Explorer I hope this will give you additional informations to help us solve the problem Best regards AttachmentProblem.zip (711 Downloads) |
1/30/2006 12:04 PM | |
Posts: 3 Rating: (0) |
Hello Nemo, AttachmentCapture Netpro Projet MSSA.zip (795 Downloads) |
Follow us on