Industry Online Support
Technical Forum
2/15/2013 11:50 AM | |
Joined: 1/23/2013 Last visit: 8/21/2024 Posts: 38 Rating: (1) |
I have PLC S7-416-2 with OSPCS7 V8.0 UPD1. (Whole plant actualy consist of 4 these PLC, each PLC has own OS, additional redundant OS servers for whole plant ) On some signals, which are connected throught ET-200M to PLC, I don't receive alarm all messages to OS. I use also my own block for graphic representation on OS and these always represent current state. Sometime happends that OS register some transitions, then two transition aren't recorded, and later is all transition recorded. I check also WinCC Chanel diagnostic and record trafic during problematic transitions but recordings are same when transition is ok. I check also that i dont' have problem with Alarm Logging\" InputQueue" (50000). What I could more check? More information:Configured communication jobs:1800, used communication job around 700. Alarms configured on Event_TS and Alarm_8p.
Attachment0.ZIP (56 Downloads) |
Last edited by: janbar_k at: 2/15/2013 11:59 AM |
|
5/11/2015 2:32 AM | |
Joined: 11/29/2010 Last visit: 7/13/2024 Posts: 3 Rating: (1) |
Hi,
|
Follow us on