Industry Online Support
Technical Forum
11/19/2009 12:49 PM | |
Posts: 40 Rating: (0) |
Hallo, i am working on a project and i would like to put sound when an alarm occur. I read in forum a way to put an alarm using a dll file(/tf/WW/en/Posts/6906) that someone create.It works great when i run the playscript by pressing a button but it doesn't work when i try to run the script via change of value of a tag. I would like to change the value of a tag inthe plc and then start the sound. Can anyone help me? |
11/19/2009 5:02 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi Geochris, did you already have a look at this FAQ: http://support.automation.siemens.com/WW/view/en/26106312 |
mfG / Best regards |
|
Follow us on