10/30/2018 12:56 PM | |
Posts: 9 Rating: (0) |
Hi, I have a number of WinCC Reports which contain an alarm view filtered by class and time. My issue is that the alarm view prints an ugly-looking box all the way down the page when no alarms are present (or in the case that alarms are present, it prints them properly but then fills the rest of the page with the box fields). I have recently updated from WinCC V13 to WinCC V15 and didn't have this problem before. I have deleted the alarm view in the report and replaced with a new one from the V15 toolbox but this didn't have any effect. It's not a major problem, but it looks untidy. Attached is a copy of a sample report (Page 3 contains the alarm view, the SQL filter is in the top right hand corner) along with screenshots of the configuration for the view. Would be grateful if someone could point out the obvious to me as it's bugging me! Thanks. Matt. Attachment1540898547_HV2_Rinse_Report 301018 1122hrs .pdf (101 Downloads) |
10/30/2018 12:56 PM | |
Posts: 9 Rating: (0) |
|
10/30/2018 12:56 PM | |
Posts: 9 Rating: (0) |
|
Follow us on