3/25/2021 6:05 PM | |
Joined: 11/8/2017 Last visit: 9/23/2024 Posts: 337 Rating: (189)
|
Hi, The only way I can think of achieving what you refer to is to run the Management Station in 'Closed Mode'. See HERE for detailed information. Running in Closed Mode places various restrictions on the OS though, and is not recommended for use on the main server, which may make make this option unsuitable for your system. It would need to run on a Client PC installation. With Desigo Insight, achieving what you refer to was fairly easy - there was a Standby user that could be configured. However, it's not the same with Desigo CC. Regards, |
Follow us on