Industry Online Support
Technical Forum
10/23/2007 10:54 AM | |
Posts: 26 Rating: (1) |
Hi all PCS7 experts!! I have a problem when filtering alarms in reports in a redundant-server structure. I have a redundant-server structure ("SRV-M")which, infact, are clients of another redundant-server structure ("OS"). So, in my pair of serversi have loaded a server data of "OS" in order to gets its pictures and alarms. In my pair of servers i have some report layouts where i show the alarms. These reports have a filter criteria to show only some of the plant alarms (alarms come from my "SRV-M" and from "OS"). These filter criteria is formatted via a C-Script. I have test it in my personal computer using PLCSim and notwired to the plant network. Then the reports i get are right. I only get the alarms that it should, so the filter i formatted with the C-scritp is right too. However, the reports i get in my servers ("SRV-M") are wrong because they show allthe alarms. It's seems like the filter is wrongly formatted, but it isn't possible because in my PC it works. Anyway, i tried with an static filter criteria and i get the same wrong reports. Furthermore, in these layouts in have change the source data to get the alarms of the other servers "OS"... and the reports i get are right. I mean, the filter criteria is applied but i need to filter the "SRV-M" alarms, not the "OS1" ones. I send you a pair of screenshots from one of my serversshowing my server data and layout configuration. I'm working with PCS7 V6.0 SP1 HF1 and WinCC 6 SP2. Any idea? T.I.A. Regards! Attachmentscreenshots.zip (365 Downloads) |
Follow us on