3/21/2013 9:41 AM | |
Posts: 4 Rating: (1) |
Dear Diwa, I have read your 7 valuable posts, Further Can you add some information about the Technology Boards(T100..T300) on the drive units, TMSK
|
7/22/2016 4:19 AM | |
Posts: 153 Rating: (7) |
great |
7/25/2016 2:57 AM | |
Posts: 153 Rating: (7) |
Very nice and helpful DIWA |
8/11/2016 6:51 AM | |
Posts: 92 Rating: (5) |
It can be ausome , what elese? |
3/27/2018 10:30 PM | |
Posts: 6 Rating: (0) |
Dear dchartier, Thanks for the PDF file. I observed though you made an error. You put Part 1in there labelled as Part 2 and therefore skipped the original Part 2. I have updated this file (See attachment below). Also, I attached another useful PDF file from a post by Tambe. These files lack pictures though. If anyone can update them with pictures, I believe this would be appreciated. Many thanks again to Diwa and Tambe. AttachmentUPDATED - All you ever wanted to know about the hardware of Siemens Masterdrives.pdf (773 Downloads) |
This contribution was helpful to1 thankful Users |
3/27/2018 10:33 PM | |
Posts: 6 Rating: (0) |
Here is the post by Tambe and the link to the thread. AttachmentTest procedure for testing thePCC card and Thyristors in Master drive units.pdf (768 Downloads) |
Last edited by: D. Erhahon at: 3/27/2018 10:34:01 PM |
|
Follow us on