4/14/2015 9:16 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (0) |
Only one passage or repeatedly over? |
4/14/2015 9:27 AM | |
Posts: 5 Rating: (0) |
The outputs would need to keep repeating this cycle as long as inputs are active. Also if input status changes, ouputs would need to react accordingly. |
4/14/2015 11:22 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (0) |
Here is a suggested solution.
AttachmentAlternating pulse generation.zip (278 Downloads) |
4/14/2015 11:53 AM | |
Posts: 5 Rating: (0) |
Wow, I'm astonished! Thank you very much. It's almost perfect for my purpose. My explanation might have been a little vague on time intervals, in the attached pdf I tried to draw a sequence diagram on input/output relations. It does not include all input/output variations. Idea is that when e.g. first output is "resting", the next output is turned on immediately. Can you still give me advice how to modify your excellent design to achieve that? Attachmentoutput sequence.pdf (311 Downloads) |
4/14/2015 12:09 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (0) |
What time shall the break time have? 15 seconds? |
4/14/2015 12:33 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (0) |
Delete the block B043. In block B042 set ON = 2 and OFF = 5. In block B044 set the parameter V1 = 15, V2 to V4 = 0. |
4/14/2015 12:41 PM | |
Posts: 5 Rating: (0) |
Works perfectly, thank you! Now it takes me probably a week to study and learn this. ;) |
This contribution was helpful to1 thankful Users |