7/17/2020 1:46 PM | |
Posts: 1 Rating: (0) |
i tryed to instal a gsd file,but the Step7 300 show me this msg >>> an update is presently not possible, in one or more step 7 applications at least one GSD file or type is being referenced How can i solve this problem ? Tks for help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/17/2020 14:09:06New subject after splitting |
|
7/17/2020 2:22 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666)
|
Hello leandro; You are trying to integrate a new gsd file in the HWConfig editor, when you get that message right? If the HWConfig shows an open project, you cannot add a new gsd file. The HWConfig editor page must be blanlk (Close project menu selection) to ensure that the actual project is not accessing infprmation from the gsd files in the S7Data/gsd directory. When the project is closed, then you should be able to add the new gsd file. See the following document for more details: How do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET? https://support.industry.siemens.com/cs/cn/en/view/2383630 Hope this helps, Daniel Chartier |
This contribution was helpful to4 thankful Users |
Follow us on