1/24/2012 2:10 PM | |
Posts: 3037 Rating: (192)
|
Hello, You generate the project new with the function " Rebuild All". You download the image of the panel new with function " reset to factory settings". How do you do an operating system update (OS update) on operator panels? Now you download the project to the panel. Tweety |
1/24/2012 4:48 PM | |
Posts: 7 Rating: (0) |
hi Tweety ...thanks, but it didn't help. I did all you told to do and same issue still. There's a small example project attached. Open it and start runtime. If you play with the dosing amount, wanted alarm woun't trig. In the other hand, error alarm by the system will react. That part is okey If you change the limit number, my own alarm will trigger... why? AttachmentSMALL EXC PROJECT.zip (34 Downloads) |
1/25/2012 12:00 PM | |
Posts: 3037 Rating: (192)
|
Hello Hessu, Your project does not work. It seems to be faulty. Ihave created a new project. You can test it with the simulator on the computer. It works fine on my computer. Tweety Attachmentbasicpanel.zip (52 Downloads) |
1/25/2012 1:23 PM | |
Posts: 7 Rating: (0) |
... even your project won't work????? Attached screen shots step by step what happens in my computer. I change the project little bit, all alarms are enabled and both tags are internal. steps: 1. runtime start 2. max limit to 50 3. attemp to change trigger value above the max limit 4. result, system error and trigger value back to zero 5. trigger value to 45 6. all good 7. changing max value to 40, below the trigger value 8. result, Tweety's own alarm event occur 9. max value back to above trigger value 10. result, too much again but trigger value frame back to normal colour Is my winCC corrupted? ...what you think? Attachmentstep by step.zip (37 Downloads) |
1/25/2012 2:19 PM | |
Posts: 3037 Rating: (192)
|
Hello, you must started my project with button of the sumilator. The tooltip of the button is "Start runtime system with simulator". See screenshot Tweety |
1/25/2012 3:19 PM | |
Posts: 7 Rating: (0) |
good point Tweety... and it works, crying out loud. What's wrong in my pc or is't software corrupted? ...if I install wincc again and we'll see what happens. |
Follow us on