11/3/2017 12:06 PM | |
Joined: 4/24/2006 Last visit: 9/24/2024 Posts: 8742 Rating: (1168) |
Hello, Have you seen this thread: how-to-get-the-resolution-of-analog-input Best regards, Wizard |
This contribution was helpful to1 thankful Users |
11/3/2017 12:32 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi isaakkis, unfortunally I didn´t found something relating the s7-1200 AI-cards, but the principle is the same like in the S7-300. Have a look: SIMATIC S7-300 S7-300 Module data so you have a resolution of 4096 steps. Represented from 0...32767 each step has 8 digits that means the smallest value above 4mA that the module can recocnize is 4mA + 8*578.7nA = 4,046296mA hope this helps, regards |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on