1/10/2012 11:29 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
You will find answer clicking above or below your post. |
1/10/2012 11:29 AM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hello atv127, Take a look at link bellow: http://support.automation.siemens.com/WW/view/en/42087579 Here you can download a library with two blocks to convert input and output 0..20mA to 4..20mA and4..20mA to 0..20mA. The library was created on TIA 10.5, but you can open on TIA V11 and the library will be converted automaticaly. |
1/13/2012 6:41 PM | |
Posts: 16 Rating: (2) |
Here is another picture of the FC in the Main OB, I don't know how to attach several files in the same replay, Best regards... |
1/18/2012 2:01 PM | |
Posts: 11 Rating: (0) |
Thank you so much, this was very helpful! |
5/3/2012 2:49 PM | |
Posts: 559 Rating: (87) |
Hellow atv127, Please update the status. Have got the solution? |
7/20/2012 4:16 AM | |
Posts: 35 Rating: (0) |
Hi, From 0-20 to 4-20 mA, the convert function is: y=1.25*x-6912, where x is count from 0 to 27648 for input and if x<5529.6 (at 4mA) assume that the sensor current circuit broken. From above, you can make your progam accordingly. I have done with that. As for the FAQ link (https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=42087579&caller=view), I dont know why but when I use the attatch lib together with ModbusRTU communication (slave), the communication is malfunction (return wrong data)....may be FC1 is conflict with some system function... |
Follow us on