Industry Online Support
Technical Forum
11/20/2012 9:20 AM | |
Posts: 2 Rating: (0) |
I have a 331-7KF02-0AB0 analog input card (8 x 12bit) set up on a test bench communicating to a PLC over profibus witha ET 200M module (IM153-1). I have one channel set up fora 4-20mA signal. From the manual I expect 0 plc units for a 4mA signal up to 27648 for a 20mA signal. However I get a reading of 64 when I apply a 4 mA signalto the card and 27712 when I apply a 20mA. As I go through the range in between I get a lot of readings that are 64 units greater than the theoretical. See attached for reference. Has anyone come across a similar issue. Thanks AttachmentC:\Documents and Settings\bmcnam01\Desktop\AIcard.pdf (101 Downloads) |
11/21/2012 1:33 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
Hello, Here it is the related FAQ which supports SteveA answer:
|
Ayman Elotaify |
|
Follow us on