6/17/2015 5:23 PM | |
Joined: 1/18/2008 Last visit: 3/20/2024 Posts: 36 Rating: (0) |
Hi Confirm the module
is configured for the correct signal input range using the configuration plug on the side. |
6/17/2015 5:35 PM | |
Posts: 1058 Rating: (93) |
Can you read out the diagnistic buffer of your cpu and post it here? It would be helpful to understand the problem.....
regards |
6/18/2015 12:58 AM | |
Joined: 6/22/2013 Last visit: 11/24/2023 Posts: 141 Rating: (3) |
The error may have been cut by the cable or can understand the problem? |
6/18/2015 8:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi diosnel, see this manual. maybe it helps you to get your problem solved. SIMATIC S7-300 S7-300 Module dataIf it not helps, give us more information about your problem, e.g. diagnostic buffer. It could also help you, when you tell us what you want to meassure with it,regards, |
FCK WAR! |
|
6/19/2015 4:24 PM | |
Joined: 6/22/2013 Last visit: 11/24/2023 Posts: 141 Rating: (3) |
if one is to bypass unused entries must be in what position the module. |
Follow us on