12/27/2018 9:41 PM | |
Posts: 121 Rating: (2) |
This produced the exact same result Thanks for trying |
12/27/2018 9:44 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197) |
No. Then make you not the same as I. |
This contribution was helpful to1 thankful Users |
12/28/2018 7:07 AM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197) |
I can not understand your devotion, something is different with you. I have set the voltage at the analog input so that the analog input after the conversion shows exactly 3222 units. The measured voltage at the analog input is 1.171 VDC (with a set measuring range of 2 VDC). Attached is an online screenshot with the values and the complete calculation. AttachmentPressure.pdf (119 Downloads) |
12/28/2018 7:55 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197) |
If yo mean... |
Follow us on