11/14/2012 3:57 PM | |
Joined: 10/31/2011 Last visit: 1/30/2024 Posts: 400 Rating: (5) |
Dear Johnluck, To apply potential on second PLC you have to synchronise zero volt of both side supply.Othr solution is to use signal isolatorhttps://www.automation.siemens.com/mcms/industrial-controls/en/control-devices-monitoring/schnittstellenwandler/pages/default.aspx?HTTPS=REDIR. Regards
|
11/27/2012 11:03 AM | |
Posts: 8 Rating: (1) |
Hi, You are right. you have to scale the 4-20ma signals properly, 4ma-0 and 20ma - 27648.hopefully your problem will be solved. |
11/27/2012 3:13 PM | |
Joined: 3/29/2012 Last visit: 10/8/2023 Posts: 61 Rating: (0) |
The problem I am actually facing is that despite the fact that i have 4-20mA at the PIW input the values i see at the input of the scaling fc FC105 is -32767 at 4mA and 32767 at 20mA. This is the value i want to scale to 0-20000. I know that FC105 do its calculation base on the following The constants K1 and K2 are set based upon whether the input value is BIPOLAR or UNIPOLAR. ·BIPOLAR: The input integer value is assumed to be between –27648 and 27648, therefore, K1 = –27648.0 and K2 = +27648.0 ·UNIPOLAR: The input integer value is assumed to be between 0 and 27648, therefore, K1 = 0.0 and K2 = +27648.0 If the input integer value is greater than K2, the output (OUT) is clamped to HI_LIM, and an error is returned. If the input integer value is less than K1, the output is clamped to LO_LIM, and an error is returned. Attached below is the snapshot of the scaling fc. thank you. AttachmentC:\Documents and Settings\ngoyedelek\Desktop\siemen.zip (46 Downloads) |
johnluck |
|
Follow us on