3/5/2021 8:44 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32993 Rating: (4078)
|
Then the value in VW0 (NAI1) is equal to 0. Did you also look at the value in VW0 with the data table?
|
3/5/2021 9:15 AM | |
Posts: 11 Rating: (0) |
Is that what you meen? |
3/5/2021 9:20 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32993 Rating: (4078)
|
No, the data table is something else. Where should the value in VW0 come from? From B009? If so, do you transfer the value from B009 to VW0 using parameter WM mapping? In attachment a video. That shows you using the Data Table in simulation. AttachmentData table.zip (194 Downloads) |
3/5/2021 9:31 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32993 Rating: (4078)
|
See attached PDF
AttachmentUntitled.pdf (177 Downloads) |
3/8/2021 9:02 AM | |
Posts: 11 Rating: (0) |
Yes Siemens KPT400 basic, mono, PN My old LSC V7 soft uploaded. Please, check the value of the analog treshold value int the simulator after downloading. The treshold trigger automatically picked up the UP/DOWN Counter start value. Thanks AttachmentV2.3.0_mod.zip (187 Downloads) |
3/8/2021 10:33 AM | |
Posts: 11 Rating: (0) |
AttachmentKomposztáló.zip (191 Downloads) |
Follow us on