7/21/2011 2:57 PM | |
Posts: 87 Rating: (1) |
only after power off.... sensor connected to station by 4..20mA(4wires) and powered before station (appr. 2..3 sec).... |
7/21/2011 3:45 PM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046)
|
Hello andrewF do you have product release 4 or 5 of the 7KF02 and is it operated behind an IM365? If so,the FAQ below may contain the answer: Why, after powering up the CPU or after changing a module, do you get an I/O access error to the analog module 6ES7331-7KF02-0AB0 and 6ES7331-7KB02-0AB0? If it is not applicable, I suggest you follow the Steps as outlined in the FAQ below: What measures do you need to take for error-free operation of the analog input modules SM331 (6ES7331-7KF02-0AB0 and 6ES7331-7KB02-0AB0)? And just in case you have a Software redundant system, the FAQ below may help too: Why are sporadically not all the modules parameterized when starting up a software redundancy configuration with 2 IM 6ES7153-2BA..-....? If all fails, I suggest you try a new AI module and should that not help send a support request to Siemens. I hope this helps |
Cheers |
|
Follow us on