Industry Online Support
Technical Forum
9/22/2008 11:02 PM | |
Posts: 672 Rating: (56) |
Hi, Have you got the password active when transfering in normal mode ? |
9/23/2008 7:50 PM | |
Posts: 14 Rating: (0) |
no i dont have password, how i use a password and where? |
9/23/2008 10:11 PM | |
Posts: 672 Rating: (56) |
HI, In normal mode press the eyeball key and 1111 "ENTER" they go back to DATA IN/OUT |
9/23/2008 10:36 PM | |
Posts: 14 Rating: (0) |
thank very much in the next time i try |
9/24/2008 8:46 PM | |
Posts: 14 Rating: (0) |
Have a little question, it's possible that without the info of the Tea1 and Tea2 file the axis borad are power off? Thanks |
9/27/2008 2:46 PM | |
Posts: 14 Rating: (0) |
For load the Plc you intend the two file TEA1 e TEA2 or the s5 program? |
9/28/2008 10:39 AM | |
Posts: 672 Rating: (56) |
Hi, Either a text file %PCP which is a hex dump of the plc, or the S5 program if you have an S5 programming device or software. |