9/13/2010 9:34 AM | |
Posts: 41 Rating: (3) |
Hi all, I have been using an S7-1200 along with the Wonderware DASSIDirect server to communicate with Wonderware Intouch. [schnippschnapp] A seperate problem, if I have a +/- 10V analog input signal I try and access for example IW96 it does some very strange things with the input goes below 0V. For 0-10V it goes from 0 to 32000 about, however when I go below 0V it jumps to 65500 and then goes down to about 33000. I am not sure if this a problem because the server cannot do signed integers? Thanks for any help in advance! Splitted from Problem with S7-1200 and DASSIDirect server. |
Last edited by: O_Moderator at: 9/14/2010 8:35 AMnew subject after splitting |
|
9/14/2010 7:06 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, I prefer to do scaling in PLC.(it's an easier way). Look at attachment. Best regards, Hristo Mihalev |
9/16/2010 4:24 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Look at attachment.(Chapter 3) Best regards, Hristo Mihalev AttachmentDasSIDirect.pdf (1039 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on