2/9/2011 9:49 AM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Hello, I recommend a convertiotore MOXA wifi RS 232 (logo )-----> LAN (WiFi) PC |
2/9/2011 12:59 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Will not work with Logo, here is a thread where you can read how to communicate over Lan, once that works succesfull at the workbench you can make it wireless. /tf/WW/en/Posts/52836#top |
Problem solved? |
|
2/13/2011 6:09 PM | |
Posts: 153 Rating: (16) |
Hi_bermuda In catalogue SIEMENS GAMMA (2010) in section Gateways, Interface Converters there is a description for KNX/SYMATIC 7, but it is required to use symatic S7 - 300. In Attachment there are pages from catalogue. I think that the given system of telecommunication will be more expensive and will contain more devices than a sheaf S7-200 +modem ---modem+S7-300 AttachmentBinder2.pdf (659 Downloads) |
2/15/2011 8:32 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Look at: http://www.plcshop.nl/ almost a LOGO! Possible the new series 0BA7?? |
2/16/2011 8:11 AM | |
Posts: 151 Rating: (3) |
hello Andres [Str] thanks for your file, but do you know how can i use profibus or asi instead of knx? thanks |
2/16/2011 11:37 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
There is noProfibus module for a Logo, for Asi have a look here: http://support.automation.siemens.com/WW/view/en/7047284 hope this helps. |
Problem solved? |
|
Follow us on