12/3/2009 6:11 PM | |
Posts: 33 Rating: (1) |
Hi, is there any way to comment an entire network in a function (equivalent in C languafe to // or /*.....*/) thanks |
12/3/2009 7:16 PM | |
Posts: 33 Rating: (1) |
I'm actually using only FBD ! |
12/3/2009 10:24 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Dear Cpt_KirK, You can add your comment on the comment area as shown in the picture. To disable the network without deleting, follow dchartier suggestion by adding bit (always off) in the begining of the network. It does not matter the language of programming you use. It works with STL, LAD and FBD too. Regards, |
Ayman Elotaify |
|
This contribution was helpful to3 thankful Users |
12/4/2009 5:53 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Just to clear up a possible source of confusion forCpt_KirK: Adding an "RLO 0" to a LAD or FBD Segment does NOT stop the scan of the network nor is it the same as doing STL "//" commenting out of code. Jumping over the LAD/FBD network OR doing a cut/paste of the network into a dummy offline block OR changing the view to STL and use "//" for every command in the network would achieve thesame though. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
12/4/2009 10:50 AM | |
Posts: 33 Rating: (1) |
Maybe in the future it would be nice to have an option to disable a network in step7 ! |
Follow us on