7/17/2014 8:35 AM | |
Joined: 7/27/2012 Last visit: 8/15/2024 Posts: 24 Rating: (0) |
Hello I have convert a S7 project to TIA. The project was a S7-300 The FC4 /FC1000 contains STL code and this is not support in the S71200 range.Is there a toll to convert it to SCL, or can some one help me to convert it. Any help and tips are welcome Thanks in advance Jan AttachmentIndex_BLKMOV_workmem.pdf (108 Downloads) |
7/17/2014 8:38 AM | |
Joined: 7/27/2012 Last visit: 8/15/2024 Posts: 24 Rating: (0) |
Here the project codeAttachmentAnyHandeler_V13.zip (114 Downloads) |
7/17/2014 3:54 PM | |
Joined: 7/27/2012 Last visit: 8/15/2024 Posts: 24 Rating: (0) |
Hello thanks for the tips Im working on it. See pdf.
AttachmentArray-udt-move.pdf (104 Downloads) |
7/17/2014 4:16 PM | |
Posts: 5225 Rating: (1192) |
It is heel goed so. Vele dank voor de nota. Greetings. w |
Follow us on