3/18/2020 3:27 PM | |
Joined: 2/1/2010 Last visit: 4/24/2024 Posts: 131 Rating: (66) |
Did you create all the s7 attributes on your custom block type for all the used IOs? I suppose you did, but just checking. If you run APDiag do you get any error messages when opening the faceplate? |
If my post helped you, please rate. Thanks. |
|
3/18/2020 3:38 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi AutoGen_1260505, you didn't connect a variable to "LinkTag3", so you didn't have the permission to operate. Normally you connect the variable OS_PermLog to "LinkTag3" and with "BitIndex4" you define the Bit which has to be TRUE that you can operated. Helpful to create your own faceplates is the manual PCS 7 APL Style Guide, there you can find the description for the most attributes like "LinkTag3" and "BitIndex4" With regards |
3/18/2020 3:52 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, What value did you set under LinkedOp->LinkOp? It should also be ".Param_Force_Value". If not set, you won't get the permission. |
Last edited by: Oreca at: 03/18/2020 15:53:12If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/18/2020 4:06 PM | |
Joined: 11/7/2019 Last visit: 4/24/2024 Posts: 17 Rating: (0) |
Oreca, LinkOP and LinkedOP are the same variables. I try to parametrize link tag3, no results. Thanks. |
3/18/2020 4:37 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
In your last picture is another variable configured. Can you show me the complete setup of Links and LinkedOp |
If I could help you, you can use the RATE button. Thank you. |
|
3/18/2020 4:43 PM | |
Joined: 11/7/2019 Last visit: 4/24/2024 Posts: 17 Rating: (0) |
Yes, here. |
3/18/2020 5:38 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Please change the value under: "OperationLevel". You forgot to add the point. Is this variable valid? Or does it need to be changed to: .Param_Force_Value#Op_Level? |
If I could help you, you can use the RATE button. Thank you. |
|