5/2/2016 1:36 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
FM458-1 is not a replacement of Add FEM. These are two different modules for two different applications. |
Last edited by: Navnag at: 5/2/2016 1:38:48 PMLast edited by: Navnag at: 5/2/2016 1:39:40 PMLast edited by: Navnag at: 5/2/2016 1:40:31 PMLast edited by: Navnag at: 5/2/2016 1:45:01 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
5/3/2016 9:33 AM | |
Posts: 18 Rating: (0) |
firstly thanks for consideration.as you told the FM module use for high performance closed loop.my question is that can FM 458 be used as redundant in s7-400H?the point is redundancy in FM module. AddFEM has implemented as turbine governer which connected to FM 458 module via profibus topology.
|
This contribution was helpful to1 thankful Users |
5/3/2016 9:45 AM | |
Joined: 8/25/2006 Last visit: 9/23/2024 Posts: 2209 Rating: (278) |
Hello. No, FM458 can not be used as redundant module. |
5/4/2016 8:18 AM | |
Posts: 18 Rating: (0) |
thanks for cleared answer. is there any solution to use as redundant structure? |
Follow us on