9/4/2019 4:01 PM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Dear EBMX3, What version of PCS 7 are you using right now? Could you attach the installed Software which available in your start menu -> siemens automation folder? And what is your station's specification? RAM, processors, Windows? What is the project size? Is it too big? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
9/5/2019 5:18 AM | |
Posts: 33 Rating: (5) |
Hi JazTai, Thanks for the reply. PCS7 version 9.0 SP2 Installed Software, please see the attached file. For the station specification, I'm using a virtual machine with 8 GB RAM, processor i7 @ 2.4GHz, Windows 10 Enterprise 2015 LTSB. For the current multi-project size, it's around 10GB. AttachmentInstalled Software.pdf (40 Downloads) |
9/5/2019 8:00 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Dear EBMX3, I guess the issue is coming from the project size. VMware might be one of the reason too causing the performance slow. Your RAM is 8GB only. For a big project like you, normally we install the system directly on a window and a good processor, SSD and 16GB RAM. At the moment, check the project folder. Are you able to optimize the project folder? I can give you some suggestions here. 1. Clean all .sav file. 2. check all pdl files that are having abnormal file size, find ways to reduce the file size. (you should be able to recognize it easily.) 3. locate the OS server SQL file, any tag logging/alarm logging archive file stored inside your project? consider doing some cleanup. 4. Did you store any big pdf file inside your project? 5. Any high definition picture/emf/ jpg stored inside your project? Resize them. 6. Locate all the big files in the projects and analyse them. you can do a time record to compare current and after clean up. Hope it can help you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on