2/11/2021 5:31 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, It could be the ES was used to download to another CPU like a test CPU and the PO were not booked back from that CPU. Or one CPU was replaced but PO were not booked back/restored |
If I could help you, you can use the RATE button. Thank you. |
|
2/12/2021 9:24 AM | |
Posts: 198 Rating: (60) |
Hello Jabbi_King, In addition to Oreca's comments, the following links will help you understand the other potential reasons for loss of AS RT PO count and how the licenses are actually counted for the AS and OS aspect: https://support.industry.siemens.com/cs/ww/en/view/38849821 https://support.industry.siemens.com/cs/ww/en/view/38855207 Hope this helps! |
Last edited by: Jen_Moderator at: 02/12/2021 12:21:04Optimized links. |
|
2/12/2021 5:11 PM | |
Joined: 1/26/2014 Last visit: 3/19/2024 Posts: 164 Rating: (0) |
If i downloaded complete program by mistakenly for two times.. Then two time POs used.. So can i Book Back all POs?? |
2/12/2021 5:37 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
That is not possible. The PO are downloaded to the CPU and maintained there. Otherwise Siemens would be very very rich As I said, there are a few possibilities that can occur with your situation. Download to test CPU and not booked back, downloaded to a CPU that was replaced and PO not booked back. Other situations like using the ES for downloading multiple projects to different PLC's can occur as well. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on