1/29/2015 3:07 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello @rturas, it is interesting to you? How do you create a WinCC flexible faceplate? |
This contribution was helpful to1 thankful Users |
1/29/2015 3:23 PM | |
Posts: 1058 Rating: (93) |
If I understand it right, you want to create some kind of faceplate with motor datas. How do you create a WinCC flexible faceplate? How do you integrate structures into faceplates? Tips and tricks for creating faceplates regards |
This contribution was helpful to1 thankful Users |
1/30/2015 9:08 AM | |
Joined: 1/27/2009 Last visit: 9/17/2024 Posts: 172 Rating: (8) |
Hello again, I have studied about faceplates yesterday and looks like they are like templates. So if i make a faceplate i gonna need to use it as many time as many motors i have, in that case i gonna need to make as many screens as many motors i want to monitor, or if i wanna use only 1 screen then i need to play with layers. If this is the only way then it is so complicated, i must say, or i missed somethingI made some screenshots how i did it on mitsubishi hmi: 2 screens and table of aliases. On the button click event i assign the same screen that will be opened but different aliases will be assigned. BR @rturas
AttachmentiX.pdf (167 Downloads) |
The only thing necessary for the triumph of evil is for good men to do nothing |
|
1/30/2015 9:27 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello @rturas Have you already seen also this: How does tag multiplexing work? How does address multiplexing work? |
This contribution was helpful to1 thankful Users |
Follow us on