1/14/2015 6:12 PM | |
Posts: 84 Rating: (19) |
Hi, Usually we all set the Network adaptor of our PC to assign an IP address automatically. Hope you all noticed that when downloading a program to a new PLC with the above setting TIA software will detect the PLC and assign a temporary IP inside the PC. This feature looks good. Once the IP is set to PLC, after we restart the PC and when we try to communicate with the PLC it will fail. So we usually set one static IP in our PC according to our PLC IP address. Once we set a static IP in our PC we not able to access the local connected server or internet unless we set to assign an IP address automatically. Siemens released a Software tool named "SIMATIC Automation Tool". This is a very useful tool for service and maintenance people to handle PLC without TIA software. I found a hidden feature of this tool. We just need to set our PC wifi or lan adaptor to assign an IP address automatically. In the software select the adaptor and scan for devices. It will scan and detect connected PLC in the network and it will internally set a temporary IP address in the PC. So we no more need to worry on setting IP address in our PC and easily can access PLC from TIA Portal Will be great if Siemens integrate this great feature in TIA Portal Software by default. AttachmentSIMATIC Automation Tool.zip (2455 Downloads) |
Last edited by: subin at: 1/22/2015 5:04 PM |
|
This contribution was helpful to3 thankful Users |
Follow us on