2/11/2009 11:22 AM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi ste_angioni, attached, some extract from the "Getting started", page 27,below: http://support.automation.siemens.com/WW/view/en/18657078 With the help of the Audit viewer you can comfortably evaluate the Audit Trail for external analysis on an Office PC. • Use the “HmiCheckLogIntegrity” DOS program: With the help of the DOS program an automatic check of the Audit Trail in Batch mode via the return values is possible. This means, usually, the viewing of the audit archive is only possible with these tools. If you like to do thisby the panel, you have to create your own viewer: http://support.automation.siemens.com/WW/view/en/24327008 |
Last edited by: The Body at: 2/11/2009 11:23 AMmfG / Best regards |
|
Follow us on