2/9/2018 1:18 PM | |
Posts: 2 Rating: (0) |
Then why is the Authors V4.5 available for download if it cannot be used? Is there a way to create an Authors V4.5 disk with no authorizations on it? |
2/9/2018 1:27 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979) |
because not on all authorization disk is authosw stored, there are disk with only the licence and then you need the authorsW program you can create a service request like described in this FAQ to get help for the problem with defective disk. https://support.industry.siemens.com/cs/ww/en/view/772175 you can also try to use AuthorsW V2.5 (windows program) and try a offline Transfer, then you need no Auth Floppy disk. Regards Christoph |
Last edited by: ChristophD at: 2/9/2018 1:29:43 PM |
|
Follow us on