6/28/2006 2:11 PM | |
Posts: 3149 Rating: (171)
|
Hi, we´ve already discussed some interesting points: /tf/WW/en/Posts/3351 nemo |
6/29/2006 11:00 AM | |
Posts: 3149 Rating: (171)
|
Unfortunately I don´t see any real "elegant" method. You should always keep in mind, that huge global scripts will slow down your system performance. nemo |
7/4/2006 1:14 PM | |
Posts: 42 Rating: (1) |
OK, stage one is complete; I am sending email with the message number automatically when a message goes active based on the 'State' portion of the structure in gMsg. Now there are two things I would like to do with this but I am unsure of how best to achieve the desired result and where to perform the additional steps: - 1, Determine whether or not to send an email message. To do this I need to be able to identify the message, either by a group name or similar technique. I think I should do this in the gMsg function as I will only trigger the emailing script when required so it should be less of a burden on the system. 2, Query the database to get message text to attach with the message number. I think I should do this in the VB script. I have attached my code so if anyone else is interested in doing the same things here it is:-
|
7/4/2006 4:27 PM | |
Posts: 42 Rating: (1) |
Thanks Salma, I'll give th code a try. |
Follow us on