6/9/2017 11:37 AM | |
Posts: 1 Rating: (0) |
A few more information about automatic creating of messages texts. According to the S7 help "/ Configuring Messages /The Message Concept / How to Generate an STL Source File from Message-Type Blocks": When you generate an STL source file from message-type blocks, the configuration information is also written to the source file. This information is written to a pseudo-comment that begins with "*$ALARM_SERVER" and ends with "*". I created a message text "Lorem Ipsum" in an instance data block of to the SFB 33 "ALARM" and I generated a source file from that block. I found out in the source file that a message text is coded in a Base64 format. So that a text "Lorem Ipsum" is "TG9yZW0gSXBzdW0=<", e.g.
It is possible to use an automatic generation of a STL/AWL source code with message-type blocks that have multilingual (many LCID) text messages. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/12/2017 12:42:07 PMNew subject after splitting |
|